The Grundfos CHB or Compact Hydro Block is the latest hydraulic platform from Grundfos, offering compact design, numerous features, easy serviceability and energy optimised design.
Since 2000, Grundfos has produced more than 6.5 million hydraulic systems. This means that we have extensive experience in designing and producing reliable, robust and serviceable solutions. Experience shows in the design and functionality of our innovative hydraulic platform.
Main features & benefits
- Fits the new EuP ready UPM2
- Pump with air vent
- Outlet thread 3/4"
- Inlet 3/4" brass mounted with a clip
- PHE CH connection primary circuit
- D10 connection on top, possibility of easy assembly and service
- Pressure switch
- Expansion tank connection
- D6 connection on side for manometer
- D10 connection on side (expansion)
- D10 bypass connection on back
- Pressure relief valve connection on top
- Plug for closing internal bypass (option: plug with connection for pressure switch or expansion)
- Bypass cartridge with check valve
- Flapper valve with stepper or synchronous motor
- Compact DCW fitting
- Fresh water connection on top (option: version with flow meter)
- PHE DCW connection
Contact us for further information at hvacoem@grundfos.com